Back to Main Menu

Using Advanced Search Profile

Introduction

The Assetic REST API allows data to be bulk exported from Assetic utilising saved profiles from the Advanced Search functionality.

There are 2 REST API endpoints:

  • GET /api/v2/search
  • GET /api/v2/search/GeoJson

The difference between the 2 endpoints is that the API endpoint GET /api/v2/search/GeoJson returns the spatial location of each record, and the whole search result is formatted as GeoJson to allow GIS applications to utilise the search result.

NOTE  The number of records returned is limited to 10,000.  The 'export' REST API endpoint may be used to export all records in the search.

Advanced Search Profiles

The first step is to save an Advanced Search Profile.  This is described in Search Basics. Configure an Advanced Search Profile that returns the required fields, including any filters that you may require to restrict the search results.

NOTE  If using /api/v2/search/GeoJson there is no need to assign additional fields in the search, the spatial data is automatically included

The API endpoints require the unique GUID identifier of the Advanced Search Profile.  To obtain this identifier simply open the Advanced Search Profile in Assetic and copy the GUID part from the URL in the browser navigation bar.  In the example screenshot below the full URL is: https://xxx.assetic.net/Search/AdvancedSearchProfile/SPDashboard/Default/ff03c4bd-4f1d-e611-9458-06edd62954d7?loadprofile=True

From this URL the GUID is: ff03c4bd-4f1d-e611-9458-06edd62954d7 

Tiles

Tiles are used on dashboards for grids and charts.  The tile may be used as the basis of a search.  Note that the GUID of the tile is not displayed on the application and requires some technical skill to obtain. 

Using the API

The API endpoints have the following parameters (common to both endpoints):

Parameter Description Type Mandatory
requestParams.id The GUID identifier for the Advanced Search Profile GUID Conditional
requestParams.sourceTileId The GUID of a system tile GUID Conditional
requestParams.page The page number to retrieve.  Default=1 Integer No
requestParams.pagesize The number of records to retrieve per page.  Default = 20, Maximum=500 Integer No
requestparams.sorts Apply a sort order to the results String No
requestParams.filters Filter the results String No

NOTE  The GUID of a search profile is normally used for searching, but alternatively the GUID of a tile may be used.  One of these parameters must be included in the request.

Page Number and Page Size

Setting page size (requestParams.pagesize) limits the number of records returned per request.  Where there are more results than specified by page size then subsequent requests can be made to the API endpoint to get the full result set.  For each subsequent request the page number (requestParams.page) specified in the parameters should be increased by 1.  The API endpoint response includes 'Total Results' which is the number of records the .

NOTE  The search does not return fields that have NULL value for all records in the response.  This means the number of fields returned by the search for a given page may be less than that defined in the Advanced Search Profile.  If multiple requests are used (to get all pages) the number of fields returned for a page may therefore vary between pages

Filters

The search results may be filtered by fields in the search.

The filter format currently supports:

  • 'Equals' which is represented by '='
  • 'Less Than' which is represented by '<' 
  • 'Less Than or Equal To' which is represented by '<='
  • 'Greater Than' which is represented by '>'
  • 'Greater Than or Equal To' which is represented by '>='

As an example, to filter by Asset Type='Sealed Road' the filter is:

 requestParams.filters=ComplexAssetType=Sealed Road

To get the field name to filter by, first run the search end point /api/v2/search/{id}/metadata, where {id} is the guid of the search profile.  The response body is a list of field mappings that map the display name visible in Assetic with the internal field name to be used in the filter, and the data type of the field.

  • {
  • "TotalResults": 2,
  • "TotalPages": 1,
  • "Page": 1,
  • "ResourceList": [
  • {
  • "Label": "Asset Asset Catalogue",
  • "Name": "ComplexAssetAssetCatalogue",
  • "Type": "System.String",
  • "_links": [],
  • "_embedded": null
  • },
  • {
  • "Label": "Asset Category",
  • "Name": "ComplexAssetAssetCategory",
  • "Type": "System.String",
  • "_links": [],
  • "_embedded": null
  • }
  • ]
  • }
  •  Dates have the format  YYYY-MM-DDThh:mm:ss where:

    • YYYY represents a 4 digit year
    • MM represents the month as a number
    • DD represents the day
    • T indicates the time follows the date.  Time is optional.  If only using date then exclude the 'T' and what follows the 'T'
    • hh represents hours on 24hour clock
    • mm represents minutes
    • ss represents seconds

    The following example shows a filter that filters by Last Modified Date greater or equal to 4th July 2016

     ComplexAssetLastModified>=2016-07-04

    A filter may include several filters, each separated by a comma.   When using multiple filters each filter is joined as an 'And', so only records that satisfy all filters will be returned.

    In the example below only records where the Asset Type='Sealed Road' that were modified on or after 4th July 2016 will be returned

     ComplexAssetLastModified>=2016-07-03T1:16:07,ComplexAssetType=Sealed Road

    NOTE  The internal field name for Asset Type is used, rather than the display name. The filter cannot be applied to all fields.

    Sorting

    The results may also be ordered via requestparams.sorts.

    The syntax is to apply the keyword 'asc' (Ascending order) or 'desc' (Descending order) to the field name, delimited by a dash ('-')

    The following example shows the syntax for ordering the results by Asset ID in Ascending order

     ComplexAssetId-asc

    The following example shows the syntax for ordering the results by Asset ID in Descending order

     ComplexAssetId-desc

    Sample Request

    The following request is used to return 500 records from the first page.

      https://[your_site].assetic.net/api/v2/search?requestParams.id={profile_guid}&requestParams.page=1&requestParams.pageSize=500 

     The GeoJson equivalent is:

      https://[your_site].assetic.net/api/v2/search?requestParams.id={profile_guid}&requestParams.page=1&requestParams.pageSize=500

     For a sample script which performs the bulk export via API, please visit this article on the Integration SDK page.

     


     

    Back to Top